May 3rd to 5th 2026
Vancouver, Canada
Mail hall, booth 951
NORD DRIVESYSTEMS is one of the industry leaders in drive technology worldwide - for mechanical and electronic solutions. In addition to our headquarters in Bargteheide near Hamburg, we are represented in over 60 countries around the world with assembly plants and service centers.
Would you like to learn more about NORD products and solutions? Then visit us in main hall at booth 951. We look forward to seeing you.
Any further questions?
Please fill out and submit the form on the right and we'd be happy to speak with you further.
NORD MAXXDRIVE® Industrial Gear Units provide high output torques from 15,000 Nm to 282,000 Nm and are perfect for use in heavy duty applications such as agitators, conveyor belt drives, mixers, mills, drums or crushers.
Industrial gear units are available as helical gear units or bevel gear units. They are constructed with the UNICASE housing which was developed by us and can accommodate large roller bearings, which guarantee a long service life. By the way: NORD is the industrial gear unit manufacturer with the world's largest industrial gear units in a UNICASE housing.
Functionality with tradition. NORD helical gear units have been produced according to the tried and tested UNICASE housing principle since the 1980s and are characterised by low maintenance and a long service life.
NORD offers complete drive solutions for mixing and agitating processes consisting of an electric motor, frequency inverter, MAXXDRIVE® gear unit, and accessories from a single source. By equipping the MAXXDRIVE industrial gear unit with reinforced bearing and flange versions (VL2/KL2 - VL6/KL6), the drive can be adjusted to maximize efficiency with varying load size. Seal-less NEMA/IEC adapters (SAFOMI) and TRUE DRYWELL sealing at the output shaft allow for operational reliability. The entire drive system is delivered as a ready-to-install unit.
The Unicase housing is a NORD development that is now one of the market standards. All gear unit elements are combined in an undivided housing. This means that there is no parting line in the housing and therefore no torque-loaded sealing surfaces. All bearing points and sealing surfaces are manufactured in a single clamping operation. As a result, NORD not only ensures maximum axis accuracy and quiet, smooth running, but also a longer service life with less maintenance.
The Endurance Package from NORD DRIVESYSTEMS is a combination of several protective measures that ensure an investment will have a long operating life. These components are designed to maintain the reliability of gear units in harsh environments.
The features include: UNICASE™ housing design, QUADRILIP™ seal system, Keyless hollow shaft with safety cover, Filter cart quick disconnects, Oil sample port, Esco 3D Bullseye™ sight glass and Donaldson T.R.A.P.™ breather
1. Drying agent filter
2. Oil sampling port
3. Quick fit filter trolley connection
4. Oil inspection glass
5. Quick disconnect filter trolley connection and oil drain cock
Primarily, the NORD ECO service shows the savings potential of your application in order to optimise energy consumption for lower CO₂ emissions as well as cost savings. Our consulting concept is based on many years of experience in the production of electric motors and cooperation with customers from over 100 industries. This accumulated knowledge is continuously incorporated into the further development of our drives so that we can offer you suitable products for application optimisation.